Technical FAQs

Ask a Question

Is the 1200A R Frame Powerpact breaker rated at 100%?

Yes. If a 1200 A 100% rated I-line breaker is required, the C5 breaker will be offered with restriction for bottom location only (as back-fed main)


CTA-ID : 2005253
Was this helpful?
What can we do to improve the information ?