Technical FAQs

Ask a Question

Is the 800A P Frame Powerpact breaker rated at 100%?

I-line C4 800 A 100% rated breaker is suitable for use in any location inside the I-line PNB, and for unit mount.


CTA-ID : 2005250
Was this helpful?
What can we do to improve the information ?