Technical FAQs

Ask a Question

What information must be provided to determine the catalog number of the joint paks on I-Line II busway?<br /><br />Are they field replaceable?

Must know:
Aluminum or copper busway
3P or 4P
Busway amperage
Feeder or Plug-in busway

or

provide the busway catalog number

Yes, joint paks are field replaceable.


CTA-ID : 2005026
Was this helpful?
What can we do to improve the information ?