Technical FAQs

Ask a Question

What is the difference between the XCSE7311 and XCSE7313?

XCSE7311 - the last digit ``1`` indicates it is a French standard device with metric conduit fittings.

XCSE7313 - last digit of ``3`` indicates it is a USA standard device with 1/2 NPT conduit fittings..

Can use the wiring diagram of the XCSE7313 for both 7313 and 7311.


CTA-ID : 2004788
Was this helpful?
What can we do to improve the information ?