Technical FAQs

Ask a Question

What is the UL rating on a QBMIK slide bar interlock?

The QBMIK is a UL Listed Circuit Breaker Accessory. UL in a circle is on a label on the device. The UL file # is E84625, Volume 8, Section 1.
This device is for mechanical interlock of any two side by side Q2, QB, QD, QG, and QJ type circuit breakers.


CTA-ID : 2004779
Was this helpful?
What can we do to improve the information ?