Technical FAQs

Ask a Question

What is the horsepower rating of a DU323RB, Series F03 safety switch?

This switch is rated for 15 HP @ 240Vac, 1-phase or 30 HP @ 240Vac, 3-phase. The HP ratings applicable for a safety switch are printed on the Wiring Diagram, located inside the front cover of the switch.

CTA-ID : 2004778
Was this helpful?
What can we do to improve the information ?