Technical FAQs

Ask a Question

Customer has the Bolted Pressure Switch and asks under what conditions can 90 degree wire be used on it at 90 degree wire ratings?

The 90 degree wire may only be used if the ampacity is based on 75 degree C wire per NEC table 310-16.

CTA-ID : 2004534
Was this helpful?
What can we do to improve the information ?