Technical FAQs

Ask a Question

What size of Allen (hex head) wrench is required for the lugs on a 150, 200 or 225 ampere Main Breaker in a QO or HOMELINE load center?

Issue:
Wiring details

Product Line:
QO and HOM LC

Cause:
Torque requirement

Resolution:
The lugs on these Main Breaker load centers use a 3/8`` Allen (hex head) wrench.


CTA-ID : 10561
Was this helpful?
What can we do to improve the information ?