Technical FAQs

Ask a Question

What type of blank fillers are used in an NH1B?

Issue:
Availability of filler plates for the obsolete NH1B circuit breaker panelboard .

Product Line:
Obsolete NH1B ciruict breaker panelboards.

Environment:
Obsolete NH1B circuit breaker panelboards sold and supported in the USA.

Cause:
Selection of filler plates for the obsolete NH1B panelboard.

Resolution:
The filler plates for NH1B interiors are obsolete and no longer available.  Consider contacting a local sheet metal fabricator for this.  






Revised 3/10/04



CTA-ID : 2005002
Was this helpful?
What can we do to improve the information ?