Technical FAQs

Ask a Question

Will a QO342M225 or QO342M225RB load center accept a QOT tandem or QO tandem circuit breaker?

No, they will not. QO 3 phase load centers do not accept tandem circuit breakers. This is a 42 space/42 circuit panel, accepting full size QO branch breakers only.

CTA-ID : 2004752
Was this helpful?
What can we do to improve the information ?