Technical FAQs

Ask a Question

Will a QO318L200G or QO318L200GRB load center accept a QOT tandem or QO tandem circuit breaker?

No, they will not. QO 3 phase load centers do not accept tandem circuit breakers. This is a 18 space/18 circuit panel, accepting full size QO branch breakers only.


CTA-ID : 2004744
Was this helpful?
What can we do to improve the information ?