Technical FAQs

Ask a Question

Will a QO327M100 or QO327M100RB load center accept a QOT tandem or QO tandem circuit breaker?

No, they will not. QO 3 phase load centers do not accept tandem circuit breakers. This is a 27 space/27 circuit panel, accepting full size QO branch breakers only.


CTA-ID : 2004747
Was this helpful?
What can we do to improve the information ?