Technical FAQs

Ask a Question

Why does the Power Consumption (kWh) meter on the ATV58 display always show 0, even after several hours of operation?

This was an issue with the earlier version firmware and has been corrected with the V5.1 firmware.
Customer will have to replace control board if they need the feature. If they order a control board today then they should get the newest firmware which allows for hour meter.

CTA-ID : 2002615
Was this helpful?
What can we do to improve the information ?