Technical FAQs

Ask a Question

Is door-n-door construction available in the a NEMA 3R NQOD panelboard?

Yes. It is only available in the following sizes:

29H x 20W x 6.5D
50H x 20W x 6.5D

This is an option in Product Selectors.


CTA-ID : 2004978
Was this helpful?
What can we do to improve the information ?