Technical FAQs

Ask a Question

Will a QO312L125G or QO312L125GRB load center accept a QOT tandem or QO tandem circuit breaker?

No, they will not. QO 3 phase load centers do not accept tandem circuit breakers. This is a 12 space/12 circuit panel, accepting full size QO branch breakers only.

CTA-ID : 2004740
Was this helpful?
What can we do to improve the information ?