Technical FAQs

Ask a Question

Are 9422 circuit breaker operators CE marked?

The Class 9422 circuit breaker operating mechanisms do not require the CE Mark as they are not stand alone products, but only turn the associated circuit breaker on and off. Therefore, it is the circuit breaker that requires the CE Mark and not the mechanism.

CTA-ID : 2001804
Was this helpful?
What can we do to improve the information ?