Technical FAQs

Ask a Question

Will a QO24L70RB load center accept a QOT tandem or QO tandem circuit breaker?

This is a 2 space/4 circuit panel that will accept a maximum of 2 QOT (QOT prefix) tandem circuit breakers. QO tandem (QO prefix) are for use only in old-style (pre 1965) non-Class CTL panels. The QO tandem breaker should not be used in the subject load center.

CTA-ID : 2005194
Was this helpful?
What can we do to improve the information ?