Technical FAQs

Ask a Question

Will a QO48M30DSGP load center accept a QOT tandem or QO tandem circuit breaker?

Issue:
Product Design Features

Product Line:
QO Three Phase Load Centers

Environment:
Mounting Tandem breakers

Cause:
Application

Resolution:
The QO48M30DSGP is a 4 space- 8 circuit generator panel, that will accept a maximum of 4 QOT type tandem circuit breakers. The QO type tandem breakers are for use ONLY in old-style (pre 1965) non-Class CTL panels QO load centers. The QO tandem breaker should not be used in this load center.


CTA-ID : 2005186
Was this helpful?
What can we do to improve the information ?