Technical FAQs

Ask a Question

How do you reset the 2510 manual starter after the overload has tripped?

Issue: How do you reset the 2510 manual starter after the overload has tripped?

Product Line: All Schneider Electric products

Environment: Products sold and used in the United States

Cause: 2510 thermal units have tripped

Resolution: Push the stop/reset button all the way in until it`s practically recessed. Then push the start button. If the unit has reset properly, the start button will stay in the depressed position.


CTA-ID : 2004953
Was this helpful?
What can we do to improve the information ?