Technical FAQs

Ask a Question

What is the part number for the main wiring harness in Design B & C size 6 Alitvar 66 drive?

52021-372-50 is the wiring harness for the new style size 6 ATV66.

Design B & C drive units were manufactured after June 1, 1998 and the 7th digit of the drive serial number DOES = 1. Design A drives use a different part.

Refer to resolution 2004942 for information on the Design A drives.


CTA-ID : 2004944
Was this helpful?
What can we do to improve the information ?