Technical FAQs

Ask a Question

What is the part number for the main wiring harness in Design A size 6 Alitvar 66 drive?

52012-532-50 is the wiring harness for the old style size 6 ATV66.

Design A drive units were manufactured before June 1, 1998 and the 7th digit of the drive serial number does not = 1. Design B and C drives use a different part.

Refer to resolution 2004944 for information regarding the Design B & C drives.

CTA-ID : 2004942
Was this helpful?
What can we do to improve the information ?