Technical FAQs

Ask a Question

What meter socket closing plate is used with the EZM113125, EZMR113125 and EZMH113125?

ISSUE:
Product Design Features

PRODUCT LINE:
EZ Meter-Pak Metering Equipment

ENVIRONMENT:
meter closing plate

CAUSE:
Installation

RESOLUTION:
Use Lexan closing plate part #29007. A metal closing plate is not available.


CTA-ID : 2004705
Was this helpful?
What can we do to improve the information ?