Technical FAQs

Ask a Question

Will a QOMB2 accept a two pole QO circuit breaker.

Yes, it will accept (1) two pole or (2) one pole QO circuit breakers.


CTA-ID : 2004932
Was this helpful?
What can we do to improve the information ?