Technical FAQs

Ask a Question

Where are the neutral assembly and equipment ground kit installed in a MA1000R circuit breaker enclosure?

The neutral assembly is mounted in the right side gutter, to the right of the circuit breaker. The equipment ground is mounted in the top left gutter.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.



CTA-ID : 2004924
Was this helpful?
What can we do to improve the information ?