Technical FAQs

Ask a Question

What does a ``SF41`` suffix on a 9070 Type T industrial control transformer (CPT) catalog number denote?

The ``SF41`` suffix on a 9070 Type T CPT catalog number denotes factory installed secondary fuse clips on the terminal block which will accommodate a 1-1/2`` x 13/32`` midget fuse.  This option is limited to single voltage secondaries.  This is shown on page 8 of the Industrial Control Transformer catalog, document # 9070CT9901.

CTA-ID : 2005396
Was this helpful?
What can we do to improve the information ?