Technical FAQs

Ask a Question

What is the part number for the blank legend plate only which would install into a ZBZ32 ?

For white lettering capability on a black or red background the part number is ZBY0101. For black lettering capability with a white or yellow background the part number is ZBY0102. Both part numbers would be an 8 x 27 mm sized blank.


CTA-ID : 2005164
Was this helpful?
What can we do to improve the information ?