Technical FAQs

Ask a Question

Does Square D offer the QOE250GFINM, but with a QO260GFI factory installed instead of the QO250GFI?

Issue:
Product availability

Product Line:
QO load centers

Cause:
Application

Resolution:
No, not as a merchandised package. Consider purchasing separate components QO24L60NRNM and QO260GFI and installed in the field.
NOTE: The QO260GFI is suitable ONLY for feeding 240Vac or 208Vac, 2 wire loads. There is no load neutral connection


CTA-ID : 2004916
Was this helpful?
What can we do to improve the information ?