Technical FAQs

Ask a Question

Where is the bus cable is marked AMP E57891, 38pf capacitance measured in the seriplex cable between what pins or wires? T

The capacitance is measured between the data line and the combination of the other 4 lines.


CTA-ID : 2004905
Was this helpful?
What can we do to improve the information ?