Technical FAQs

Ask a Question

Can I use the same address for Seriplex two cards and use only some channels on each board?

Yes, you can use 2 boards with the same address and different channels on each card. However you will lose response time.


CTA-ID : 2004903
Was this helpful?
What can we do to improve the information ?