Technical FAQs

Ask a Question

What is the Terminal Lug Data for a HU464, Series F05 Heavy Duty safety switch?

The lugs on this device will accept (1) #6 AWG - 300 kcmil aluminum or copper conductors per phase. However, wire bending space available in the switch restricts the conductors to (1) 250 kcmil maximum.

CTA-ID : 2004897
Was this helpful?
What can we do to improve the information ?