Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H364, Series F05 Heavy Duty safety switch?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Terminal Lug data

Cause:
Installation

Resolution:
The lugs on this device will accept (1) #6 AWG - 300 kcmil aluminum or copper conductors per phase. However, wire bending space available in the switch restricts the conductors to (1) 250 kcmil maximum.


 
Was this helpful?
What can we do to improve the information ?