Technical FAQs

Ask a Question

What are the standard lugs used with NA/NAL/NC/NCL/NX/NXL/NE/NEL 1200 amp frame breakers?

AL1200NE6 which accept 4-#3/0 AWG - 600kcmil per phase. There is one lug in each kit.


CTA-ID : 2004668
Was this helpful?
What can we do to improve the information ?