Technical FAQs

Ask a Question

Is there a mounting kit for the SDSA1175 Secondary Surge Arrestor?

Issue:
Is there a mounting kit for the SDSA1175 Secondary Surge Arrestor?

Product Line:
Surge protection.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The SDSA1175 can be mounted through any standard 0.50`` conduit knockout. The actual hole size is .875``. A mounting kit, QOSAMK, is also available for mounting the SDSA1175 internally in a QO or HOMELINE, Series G1, G2, S1 or S2, single phase, 100 - 225 ampere convertible main, main breaker load center.


CTA-ID : 2005368
Was this helpful?
What can we do to improve the information ?