Technical FAQs

Ask a Question

Are the timed contacts on an 8501 X timing attachment field convertible?

Yes. The timing attachment uses the same standard contact cartridges as the 8501 X relay and they are field convertable normally open to normally closed and normally closed to normally open.

CTA-ID : 2005367
Was this helpful?
What can we do to improve the information ?