Technical FAQs

Ask a Question

What is the part number for a legend plate with special engraving for the XB2 operators?

Use the following part numbers and specify text:
ZB2BY2002 is a 30 x 40 mm legend black with white letters
ZB2BY2004 is a 30 x 40 mm legend red with white letters
ZB2BY4001 is a 30 x 40 mm legend white with black letters
ZB2BY4005 is a 30 x 40 mm legend yellow with black letters.

Text is limited to 2 lines of 11 characters each.



CTA-ID : 2002109
Was this helpful?
What can we do to improve the information ?