Technical FAQs

Ask a Question

Are the EZM branch devices suitable for top and bottom feed?

Yes, the branch circuit conductors can exit through the top, bottom or back walls of an EZM branch device.
NOTE: For conduit entry above live parts, use UL listed raintight or liquidtight hubs.

CTA-ID : 2004146
Was this helpful?
What can we do to improve the information ?