Technical FAQs

Ask a Question

From what material is a H Hub made?<br /><br /><br />

The H Hubs are die cast zinc. The H Hubs with a CP suffix are also die cast zinc, with a nickel-chrome plating.


CTA-ID : 2004137
Was this helpful?
What can we do to improve the information ?