Technical FAQs

Ask a Question

Are NEMA 3R enclosures available with a Yale lock?

No. The Yale 511S lock is only available on NEMA 1 trims.


Revised 3/29/04



CTA-ID : 2004133
Was this helpful?
What can we do to improve the information ?