Technical FAQs

Ask a Question

Are the FCL, FHL, FAL thermal magentic breakers field adjustable? <br />

No. They have fixed magnetic settings.

The thermal magnetic breakers that are over 100a frame size are field adjustable.


CTA-ID : 2003863
Was this helpful?
What can we do to improve the information ?