Technical FAQs

Ask a Question

What bus bar material is supplied with EZ METER-PAK Metering Equipment?

Issue:
Product design features

Product Line:
EZM Metering

Environment:
Bussing material

Cause:
Application

Resolution:
EZ METER-PAK mains and branch units are designed to meet UL67, and are listed as modular panelboards. Bus bar sizes and material types are determined based on Heat Rise Testing. Square D reserves the right to use either aluminum or copper current carrying conductors to comply with this standard. See the current Square D/SE on-line digest for main bus material of each catalog number. 

 
Was this helpful?
What can we do to improve the information ?