Technical FAQs

Ask a Question

What is the Terminal Lug Data for a HU368, HU368R or HU368AWK Heavy Duty safety switch?

Product Feature

Product Line:
Safety Switch

Clarifying lug wire range

The lugs on these switches will accept (4) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase.

CTA-ID : 2003595
Was this helpful?
What can we do to improve the information ?