Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H228N, H228NR or H228NAWK Heavy Duty safety switch?

The lugs on this device will accept (4) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase and neutral.


CTA-ID : 2003587
Was this helpful?
What can we do to improve the information ?