Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H328 type safety switches?

Issue:
Wire range usable on the lugs provided.

Product Line:
HD Safety Switches

Environment:
Installation

Cause:
Wire size to be used

Resolution: 
The lugs on this device will accept (4) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase.
Alternate compression lug kit H12LKE2 is also available for this device. 

More on Safety Switches here.
Was this helpful?
What can we do to improve the information ?