Technical FAQs

Ask a Question

Do the EZM Main Fusible Switch devices come standard with lugs from the factory?

Issue:
Product Design Features

Product Line:
EZM Metering

Environment:
Main lugs

Cause:
Installation

Resolution:

The EZM Main Fusible Switch devices with the suffixes FS, FSB and FST are supplied with factory installed lugs. The EZM Main Fusible Switch devices with a FSU or FSE suffix are supplied with lugs landing pads. The U or E in the suffix of the catalog number indicates that the device meets EUSERC standards. EUSERC requires factory supplied lug landing pads to accept field installed lugs.


CTA-ID : 2004390
Was this helpful?
What can we do to improve the information ?