Technical FAQs

Ask a Question

What is the number of non-insulated jumpers in the AB1AL4?

It is 70. They are sold in packages of 10.


CTA-ID : 2004115
Was this helpful?
What can we do to improve the information ?