Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a H363AWA safety switch?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
The Equipment Ground Kit is provided factory installed in this device. Two lugs are provided, each accepting (1) #12 - 1/0 AWG aluminum or (1) #14 - 1/0 copper ground conductor.


CTA-ID : 2004114
Was this helpful?
What can we do to improve the information ?