Technical FAQs

Ask a Question

Are alternate lugs available for a MP55125, MPR55125 or MPH55125 Meter-Pak device?

Issue:
Product accessories

Product Line:
MP Meter Pak

Environment:
Main Lugs

Cause:
Wire sizes

Resoution:
Yes, alternate lug kits are available. Use MMLK500 for (2) #3/0 AWG - 500 kcmil aluminum or copper conductors per phase and neutral. Use MMLK600 for (2) #2 AWG - 600 kcmil aluminum or copper conductors per phase and neutral. One lug kit required to convert both phase and neutral lugs on one Meter-Pak device.


CTA-ID : 2003818
Was this helpful?
What can we do to improve the information ?