Technical FAQs

Ask a Question

Are alternate lugs available for the 200amp meter socket, MP, MPR and MPH Meter-Pak devices?

Current Design Meter Pak alternate lugs

Product Line:
MP Meter Pak

alternate lugs


Yes, alternate lug kits are available ONLY for the current design 200amp Meter Socket, Meter Pak devices. So depending on the catalog and series number of the meter-pak, the below lugs are available:
  1. Use the lug kit MMLK500 for (2) #3/0 AWG - 500 kcmil aluminum or copper conductors per phase and neutral.
  2. Use the lug kit MMLK600 for (2) #2 AWG - 600 kcmil aluminum or copper conductors per phase and neutral. (Note: One lug kit required to convert both phase and neutral lugs on one Meter-Pak Device.)
  3. To meet EUSERC standards, order and install alternate lug landing pad kit MMSK2, and order compression lugs separately. The MMSK2 lug pads are supplied with (2) 1/2"-13 Studs per pad on 1-3/4" centers and keps nuts for per NEMA standards.
If unsure which lugs your device accepts, contact 1-888-778-2733.
Was this helpful?
What can we do to improve the information ?