Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H328N, H328NR or H328NAWK Heavy Duty safety switch?<br />

The lugs on this device will accept (4) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase and neutral.

CTA-ID : 2003563
Was this helpful?
What can we do to improve the information ?