Technical FAQs

Ask a Question

What is needed to replace two lengths of AP308G10 in a busway run?

The AP2308G will have to be used as replacement busway. This requires at least one adapter, if not two. The adapter number is AF2308G12B or AF2308G12S. The adapter ending in ``B`` must connect to a slotted busway end. The adapter ending in ``S`` must connect to a bolted busway end. The adapters are 1 foot in length each. Be sure to allow for the adapter length in figuring the footages of new I-Line II busway.


CTA-ID : 2004381
Was this helpful?
What can we do to improve the information ?